cancel
Showing results for 
Search instead for 
Did you mean: 

Interrupts

sbivens
Associate II
Posted on July 12, 2005 at 19:24

Interrupts

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
sbivens
Associate II
Posted on July 12, 2005 at 19:24

This is from page 42 of ST10F269 USER’S MANUAL:

Controlling Interrupts

Software modifications (implicit or explicit) of the PSW are done in the execute phase of the respective instructions. In order to maintain fast interrupt responses, however, the current interrupt prioritization round does not consider these changes. For example an interrupt request may be acknowledged after the instruction that disables interrupts via IEN or ILVL or after the following instructions. Time critical instruction sequences, therefore, should not begin directly after the instruction disabling interrupts, as shown in the example.

INT_OFF: BCLR IEN ; globally disable interrupts

IN-1 ; non-critical instruction

CRIT_1ST: IN ; start of non-interruptible critical

; sequence

. . .

CRIT_LAST: IN+x ; end of non-interruptible critical

; sequence

INT_ON: BSET IEN ; globally re-enable interrupts

It makes no mention of the interrupt disable problem and indicates that only one nop is necessary.

I would hope that there is better source of information on this topic!

I did not intend to start a new topic.

:(

[ This message was edited by: Shep on 12-07-2005 22:57 ]

[ This message was edited by: Shep on 12-07-2005 23:00 ]