2026-05-15 7:55 AM
Hello,
I'm working with the STM32MP135F-DK kit and I'm trying to understand the correct way to configure interrupt lines (IRQs) for external devices, specifically for the STPMIC1 in OP-TEE.
I have been reading the official documentation and I'm a bit confused about whether it is mandatory to use the dedicated PWR Wake-up pins (WKUP1–WKUP6) for interrupt lines, or if any GPIO can be used.
---
What I observed in the reference DTS files:
Looking at the OP-TEE device tree (core/arch/arm/dts/stm32mp135f-dk.dts, tag 4.0.0-stm32mp),
I can see that all IRQ consumers use EXTI lines above 55:
- STPMIC1 interrupts-extended = <&exti 55 IRQ_TYPE_EDGE_FALLING> (WKUP1 / PF8)
---
My questions
Is it mandatory to use one of the 6 dedicated WKUP pins (EXTI 55–60) for any device IRQ managed by OP-TEE?
We’re moving the ST Community to a new platform to give you a better and more reliable community experience.