2025-07-29 8:21 AM
Hi !
We're testing with the eval-boards NUCLEO-H7S3L8 + X-NUCLEO-67W61M1.
The software is the CLI project of the NUCLEO-H7S3L8.
At the bottom of this post you will find infos to the software versions.
There we're having an issue when we try to connect to an WiFi AP and the password includes a comma (',').
It looks the ST67W6X_Network_Driver is encoding and sending the AT-command correctly, but the NCP (ST67W611M1) response with ERROR.
So it seems to us it's an issue of the NCP firmware.
Via Shell/CLI we initiate the connection to the WiFI AP via the command wifi_sta_connect.
When we set the password at the AP to "pw123456" we can connect to the AP.
When we set the password at the AP to "pw123,56" we can not connect to the AP.
For debugging we followed the code in the ST67W6X_Network_Driver till function W61_AT_Common_SetExecute(..).
There the AT-command is sent and the response is received.
If the password is not including a comma, it is connecting to the WiFi AP successfully.
The communication of the AT-command and response looks like this:
AT+CWJAP="Test_SSID","pw123456",,0
OK
If the password includes a comma, it's not working, and an error occurs.
The communication of the AT-command and response looks like this:
AT+CWJAP="Test_SSID","pw123,56",,0
ERROR
The ST67W6X_Network_Driver logs the following:
[ERROR] [469363] [shell_task] (w61_at_common.c:67) ParseOkErr Status : ERROR
[ERROR] [469363] [shell_task] (main_app - CLI.c:527) [ERROR] in W6X_WiFi_Connect API
Please can you confirm this issue ?
Additionally we're currently selecting components for a new product and we wanted to use the ST67W61M1.
So we need to know if and when this problem will be resolved ?
Thank you !!
BR
Moscht
--------------- Host info ---------------
Host FW Version: 1.0.0
Host FW Name: ST67W6X CLI
--------------- ST67W6X info ------------
ST67W6X MW Version: 1.0.0
AT Version: 1.0.0.1
SDK Version: 2.0.75
MAC Version: 1.6.38
Build Date: May 20 2025 23:01:38
Solved! Go to Solution.
2025-12-22 1:45 AM
Hi moscht,
As you may have seen in the latest 1.1.0 and 1.2.0 X-CUBE-ST67W61 releases and the accompanying documentation (for example, see the warning here), the escape mechanism is not included in X-CUBE because this could cause the SSID or password to reach the maximum size unnecessarily. It is not recommended to use special characters in SSIDs and passwords. If this required in the targeted application, the user must insert the escape character (\).
Best regards,
2025-07-29 8:41 AM
Seems that this is a not-uncommon issue; eg,
https://www.reddit.com/r/worxlandroid/comments/1chx9ja/special_characters_in_the_wifi_password/
2025-08-19 3:27 AM
Hello Moscht,
I reproduced the same behaviour on my setup. I found out that the connection is ok if the comma is preceded by a backslash. call CLI wifi_sta_connect command with "pw123\,56" as a password.
I am checking internally for what to do next. I'll feedback here when I get a status.
Best regards,
Tarik
2025-08-19 5:41 AM
Hi Tarik,
after a while with no response here, we opened a case at the ST customer support (case#: 00240171).
There we got the same answer for a workaround.
We also got this info: "For an official solution in the drivers, I'd see it possible in the next package release, scheduled to be released in a few months."
BR
2025-12-22 1:45 AM
Hi moscht,
As you may have seen in the latest 1.1.0 and 1.2.0 X-CUBE-ST67W61 releases and the accompanying documentation (for example, see the warning here), the escape mechanism is not included in X-CUBE because this could cause the SSID or password to reach the maximum size unnecessarily. It is not recommended to use special characters in SSIDs and passwords. If this required in the targeted application, the user must insert the escape character (\).
Best regards,