2003-07-21 10:07 AM
2011-05-17 2:55 AM
Hello
My boot is from the Second Flash and i want to load another program to the Primary Flash from the RS232 - for this i need to use the IAP feature but i don't find any information about this for the uPSD . The only information available is for PSD and this is not the same . Pl's advice support . Latino from Israel2011-05-17 2:55 AM
Currently we do not have IAP code written for the uPSD family. You will have to develop your own IAP code. We already have a few customers got their IAP code working. They all used the IAP code written for our DK900 eval board as a starting point and modified it to work with the uPSD. AS you know, DK900 eval board uses a standard 8032 MCU and a similar kind PSD as the one used on the uPSD.