2004-02-19 3:49 AM
2004-02-19 2:04 AM
Hi everyone!!
I've tried to make an IAP with my ST72F521R9T but it doesn't work... Is someone able to help me?? Here is the sample of code I m using...I use HdFlash.c drivers and ST7 Software library. unsigned int *nptest1; // nptest1 point on the adress VgenCalib=0x00E001 nptest1=(unsigned int*) VgenCalib; //ucConfig is a value from a dipswitch plug on my ST7 (port B) while(~ucConfig&0x40) { RASS_Disable(0x56,0xAE); // The function Vpp_Enable set a bit of a port to ''1''. // This value, tanks to a hardware design, force pin Vpp to //12-13V Vpp_Enable(); // Write the value 0x19 at the address VgenCalib = 0x00E001 HDFlashWriteByte(0x19,VgenCalib,1); // Thanks to Vpp_Disable function, Vpp pin = 5V. Vpp_Disable(); ucConfig=~PBDR; } while(~ucConfig&0x20) { // Display the value on the leds LED_vDisplay(*nptest1); ucConfig=~PBDR; } When I measure the value of the Vpp pin, it is equal to 12-13V when the program is in the first loop, and 5V when it is out of the second one.. But the value displayed on the leds is not equal to 0x19 but 0xFF... Have I made a mistake in my program or is there something I have forgotten to read in an application note?? Thanks for answering. Best Regards. Vianney2004-02-19 3:49 AM
Remember you have to erase the sector before you program it.
What return value are you getting from the ECMD register? Regards sjo