cancel
Showing results for 
Search instead for 
Did you mean: 

I use M24C64WMN6TP(8 pin package) for audio product. I want to set chip enable to 000. Therefore, it is necessary to ground the E0, E1, E2 terminals to GND. If all the E0, E1 and E2 terminals are open, will it be recognized as 000?

NShim.1
Associate

It's working fine now.

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Please have a look at the datasheet:

"These inputs must be tied to VCC or VSS, to establish the device select code as shown in Figure 3. When not connected (left floating), these inputs are read as low (0,0,0)."

Does it answer your question?

:smiling_face_with_smiling_eyes:

Best regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Please have a look at the datasheet:

"These inputs must be tied to VCC or VSS, to establish the device select code as shown in Figure 3. When not connected (left floating), these inputs are read as low (0,0,0)."

Does it answer your question?

:smiling_face_with_smiling_eyes:

Best regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.
NShim.1
Associate

Thank you for your quick response.

My question is solved.