cancel
Showing results for 
Search instead for 
Did you mean: 

What is the thermal resistance (Junction to ambient) for M95320-DRMN3TP/K

SHIRE.1
Associate
 
This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

Let's estimate some figures:

In the datasheet you'll find a maximum supply current of 5mA @ 5.5V and 20MHz = 27.5mW.

This power would lead to a temperature difference of 5.5K if we assume a (really, really bad) value of 200K/W.

Reading the whole content of a 32Kbit EEPROM at 20MHz would take about 2ms or so, after that it typically goes to standby with max 5µA = 27.5µW, which then generates a negligible increase in temperature.

Have you got any good reason that someone provides the exact thermal resistance of such an EEPROM?

Kind regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

2 REPLIES 2
Peter BENSCH
ST Employee

Let's estimate some figures:

In the datasheet you'll find a maximum supply current of 5mA @ 5.5V and 20MHz = 27.5mW.

This power would lead to a temperature difference of 5.5K if we assume a (really, really bad) value of 200K/W.

Reading the whole content of a 32Kbit EEPROM at 20MHz would take about 2ms or so, after that it typically goes to standby with max 5µA = 27.5µW, which then generates a negligible increase in temperature.

Have you got any good reason that someone provides the exact thermal resistance of such an EEPROM?

Kind regards,

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

Thank you

Peter