2007-05-07 11:34 PM
How to get a 5V output with STR750 EVAL
2007-04-27 1:07 AM
I'm using STR750 Eval board and the example : STR75xStdLib/example/GPIO.
Of course I changed this (instead of 3V3) : /* GPIO pins optimized for 5V operation */ MRCC_IOVoltageRangeConfig(MRCC_IOVoltageRange_5V); Then : /* P2.19 and P2.18 in Push Pull mode */ GPIO_InitStructure.GPIO_Mode = GPIO_Mode_Out_PP; GPIO_InitStructure.GPIO_Pin = GPIO_Pin_18 | GPIO_Pin_19; GPIO_Init(GPIO2, &GPIO_InitStructure); GPIO_Write(GPIO2, 0x00); ----------------------------------------- I get a 3.3V output on 2.19 (CN7). ----------------------------------------- What's wrong ? Is there a mask to change ? I'm using a power supply jack (5V). JP1 : PSU and DTB fitted. JP3 : CPU_3V3 fitted. JP4, JP5, JP6 : not fitted. Thank you in advance.2007-04-27 4:14 AM
Hello Xavio,
I think that you have made a misunderstanding about 5Volts subject. STR75x from ST is 5 Volts tolerant this does not mean that It will output 5volts but it Handles 5 Volts inputs and the output is always 3.3Volts. If you are interesting to have 5 Volts output, you can use the STR73x series from ST which I found the only ones within the ARM7 micros in market able to drive directly 5volts outputs. I hope this may help you and make things more clear :-] bR, Rave2007-04-27 8:21 PM
STR750 can operation as either a 5 volt or 3.3 volt device, the I/O output will be at the supply voltage level minus a diode drop.
The only difference on the schematic between 3.3 (Scheme 1) and 5.0 (Scheme 3) is providing 5 instead of 3.3 volts. I choice to use the 735 device when I started (before the 750 was available) so I can't help you without looking into the library. Could you please post the answer when you discover the problem. Barry2007-04-28 3:55 AM
Well, i'm still confused... especially when I look at this scheme 3 :
2007-05-01 8:23 PM
Well, I can't find a solution.
Barry, are you sure that it's possible to get a 5V output with the STR750 Eval ? Rave said that it's not possible... I'm still trying, I don't want to design another board :p -Xavier2007-05-07 11:37 AM
I went to a semimar when they were presenting the device and that what they indicated. The USB could not be used at 5 volts. That was the only difference. Can I say with 100%, NO, but everything that I read indicates, YES.
I choose to go with the 735 part, because KEIL at that time has simulation for all the on-chip peripherals for the 73x and not the 75x family, and I needed the additional I/O at 5 volts. Have you tried contacting ST Tech Support. They are suppose to be moniting this site, but its looks like there not. Barry2007-05-07 11:34 PM
Hi all,
Well, I haven't seen that the STR75x can operate in Dual Supply with (scheme3). Here attached the confirmation that you can have a minimum I/O output at (VDDIO- 0.8) from STR75x Datasheet : So , Yes it is possible. However, if you have the STR750-EVAL from STMicroelectronics, It seems that the scheme3 is not implemented and you have to rework the board or to design your own board with Scheme3 model to have 5 Volts Outputs. BR, Rave ________________ Attachments : my.JPG : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HtG5&d=%2Fa%2F0X0000000aKn%2FuLX54vvr4cvPSRiMvS0NHKFnuqW3CT39319cUfIiQak&asPdf=false