cancel
Showing results for 
Search instead for 
Did you mean: 

How to Drive a Stepper Motor Using STM32CubeMX and a Stepper Driver

max29
Visitor

Hi everyone,

I'm currently working on a project involving a stepper motor controlled by an STM32 microcontroller, and I wanted to share a quick overview of how I set it up using STM32CubeMX.

Hardware:
STM32F103C8T6 (Blue Pill)
Stepper Motor (28BYJ-48)
Stepper Motor Driver (ULN2003 or A4988)
Steps I Followed:
STM32CubeMX Configuration:

Created a new project for my STM32 board.
Enabled GPIO outputs for the control pins connected to the driver.
Set up a Timer for delays or PWM (if using A4988).
Generated code with HAL libraries.
Coding in STM32CubeIDE:

Wrote a simple function to send step pulses and direction signals.
For A4988, I toggled the STEP pin with a delay and used the DIR pin to control direction.
For ULN2003, I used a stepping sequence on 4 GPIO pins.
Testing:

Got the motor running with basic forward and reverse motion.
Planning to implement acceleration profiles and microstepping next.
Let me know if anyone needs sample code or has tips on improving the motion control. Also, is anyone using FreeRTOS with stepper motors?

0 REPLIES 0