Posted on May 17, 2011 at 12:03Hi All, I am not sure if anyone from ST had looked at my post couple weeks ago regarding the MCU got burned when using the Flash link. I have not got any responds. It seems I am not the only one is having this problem....
Posted on May 17, 2011 at 12:03Hi All, I am having the same problem and posted a message couple weeks ago and has no responds from any body. This is very serious problem can somebody please help?
Posted on May 17, 2011 at 12:03Hi All, I am not sure if anyone had this problem, but it happens to us twice. We have built 4 test boards using the uPSD3254BV-24U6. We were able to program the MCU without problem, however, just yesterday, we fired up...
Posted on May 17, 2011 at 12:01Hi All, I am using the uPSD3254BV and AVREF is connected to VCC with a 4.7K current limited resister. All the ADC (ADC2 and ADC3) input signals are less than 3.3V (AVREF). However, when we set the ADC input to 2.3V the...
Posted on May 17, 2011 at 12:00Hi, Thanks for the respond. Now, we go back to my original mapping, which are: RS0 0x0200 -> 0x7FFF (data space) CSIOP 0x0100 -> 0x01FF FS0 0x8000 -> 0xFFFF (program & data space) FS1 0x8000 -> 0xFFFF (program & data s...