2005-08-28 11:41 PM
2005-04-07 10:29 PM
I tried to compile a new loader for my stpc evaluvation kit as per the instruction in the .pdf file provided.
The platform was Red hat linux 9.0 The compiler was gcc version 2.6 But iam getting the following error message [root@sar10 stpckit.v.2.1]# ./build linux gcc -c -I./include -I./src/libosal/loader -I/usr/lib/gcc-lib/i386-redhat-linux/3.2.2/include -D__KERNEL__ -Di486 -O2 -nostdinc -nostdlib -fno-builtin -Wall -o src/loader/linux/linux.o src/loader/linux/linux.c In file included from src/loader/linux/linux.c:9: include/sdram.h:76:1: warning: ''/*'' within comment gcc -x assembler-with-cpp -DASSEMBLY -E startup.S > tmp.s gcc -o startup.o -c tmp.s rm tmp.s gcc -nostdlib -r -o linux.o startup.o ./src/loader/linux/linux.o lib/loader.a /usr/lib/gcc-lib/i386-redhat-linux/3.2.2/libgcc.a gcc -nostdlib -nostartfiles -static -o linux.bin -T script.ld linux.o /usr/bin/ld: warning: cannot find entry symbol _start; defaulting to 00080000 linux.o(.text+0x4d88): In function `HWIDE_IDETimings': : undefined reference to `getchar' linux.o(.text+0x4de0): In function `HWIDE_IDETimings': : undefined reference to `getchar' linux.o(.text+0x4e38): In function `HWIDE_IDETimings': : undefined reference to `getchar' linux.o(.text+0x4e90): In function `HWIDE_IDETimings': : undefined reference to `getchar' linux.o(.text+0x4ee6): In function `HWIDE_IDETimings': : undefined reference to `getchar' linux.o(.text+0x4f34): more undefined references to `getchar' follow collect2: ld returned 1 exit status make: *** [linux.bin] Error 1 [root@sar10 stpckit.v.2.1]# please help me with this2005-04-19 2:27 AM
the tool chain should be examined.
binutils and gcc should be checked.. for it. i think both or wither one of binutils and gcc is the problem. do not eager to upgrade a single tool. the toolset in harmony is a 'blessing'.2005-08-28 11:41 PM
Thanks for your reply