2006-09-12 8:28 PM
2011-05-17 12:32 AM
Hi,
I have some problems with the GPIOs when I use them as outputs with a Pull down of 100K. When I configure a GPIO as output and switch the pin to High state an then a reset event on the RESET_IN Pin occurs, I measure about 2,1V on the pin instead of an expected Low Level. When the application starts again after the Reset event I can measure the 2,1V until the application configures the GPIO again as an output. Are the any specifications concerning the Leackage current of the GPIOs (I’m using an STR912FW44X6 labeled KOR HP 619) or other ideas ? Thank you, wallie