2004-04-01 11:43 AM
2011-05-17 2:59 AM
with the emulation board with the uPSD3334, when I download the flash, where is recorded this flash, in the primary flash or in the second or where ?
2011-05-17 2:59 AM
If you are using PSDsoft to program your flash, it depends on your settings. Go to the ''Merging of MCU or DSP firmware with PSD'' settings. There you will find each ''Memory Select Name'' and an optional ''File Name'' associated with it. If the ''File Name'' field contains a hex file name, then the flash memory associated with the ''Memory Select Name'' will be programmed.