cancel
Showing results for 
Search instead for 
Did you mean: 

First problem solved, new one to fix!

jps
Associate II
Posted on March 22, 2009 at 06:08

First problem solved, new one to fix!

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
jps
Associate II
Posted on March 22, 2009 at 06:08

I've solved my first problem! As I was migrating from SOFTEC InDart with specific STVD7 to RAISONANCE R-Link with standard STVD7, I get a lot of trouble because of the settings! In fact I was not using the right s19 file! Now I can program but still not debugging! I've to spend time to read the ST help files!

New problem, I'm discovering ST7FOX and it's specific features, for example the pull-up inputs that comes mandatory with an interrupt! I've do my hardware as if I was using ST7LITE19 so no hard pull-up!

2 solutions :

1- I place pull-up resistors (difficult on my card already existing and very compact) and I set inputs as floating inputs whitout interrupt!

2- I find the way to disable external interrupt by software but keeping the Lite Timer interrupt (I use it to create a time base)!

If someone have any idea on how to do that with the FOXK1 you're welcome!

Regards

whitebull