cancel
Showing results for 
Search instead for 
Did you mean: 

Drive LCD with GPIO

alanlai1
Associate II
Posted on November 12, 2003 at 04:24

Drive LCD with GPIO

This discussion is locked. Please start a new topic to ask your question.
5 REPLIES 5
alanlai1
Associate II
Posted on November 06, 2003 at 02:44

I browsed some old-posts, and found that we can drive LCD with GPIO, mentioned a AppNotes AN104, but I cannot find it.

Can I have some trips? Thank you very much .^_______^
jatin
Associate II
Posted on November 06, 2003 at 03:04

Yes, it is possible to drive an LCD using the General purpose I/O ports.

At present, Application note available is AN1048 downloadable from the same site.

In this app note, demo software is driving a duplex LCD drive.

For your information, a new app note is coming up with the software driving Quadruplex LCD drive and with good features.

What is your application??

[ This message was edited by: Jatin on 06-11-2003 07:35 ]
alanlai1
Associate II
Posted on November 07, 2003 at 05:23

That's a Simple Clock, with alarm function. ^_^

Dear all, Thank you very much !!_^
jatin
Associate II
Posted on November 07, 2003 at 08:43

I hope you are using a LCD glass but not the LCD Module(having onboard LCD hardare driver).

If you are using LCD module then i have a software for it also to drive it using ST7.

Please let me know...

[ This message was edited by: Jatin on 07-11-2003 13:14 ]
alanlai1
Associate II
Posted on November 12, 2003 at 04:24

LCM is simple than LCD, but it is expemsive,

So we will use LCD.

^__^ thank you