cancel
Showing results for 
Search instead for 
Did you mean: 

d3nc6067s452 ? Is there an alternative?

SShel.1
Associate

I've located a part which is over heating and need to replace? Is there an alternative or is this part still available anywhere ​

This discussion is locked. Please start a new topic to ask your question.
1 ACCEPTED SOLUTION

Accepted Solutions
Peter BENSCH
ST Employee

It's the STD3NC60, which is obsolete since a long time.

You could try to replace is with a n-channel FET in TO252, >=600V, <2.2Ohms, faster than 14...19ns, >3.5A, like the STD6N60M2 or the STD5N65M6.

But keep in mind, overheating does not necessarily mean that the FET is defective, but rather overloaded. It might be a good idea to check the circuitry around it.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.

View solution in original post

1 REPLY 1
Peter BENSCH
ST Employee

It's the STD3NC60, which is obsolete since a long time.

You could try to replace is with a n-channel FET in TO252, >=600V, <2.2Ohms, faster than 14...19ns, >3.5A, like the STD6N60M2 or the STD5N65M6.

But keep in mind, overheating does not necessarily mean that the FET is defective, but rather overloaded. It might be a good idea to check the circuitry around it.

Good luck!

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.