cancel
Showing results for 
Search instead for 
Did you mean: 

Convert existing RS232-communication to USB

info80
Associate II
Posted on February 23, 2006 at 12:57

Convert existing RS232-communication to USB

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
info80
Associate II
Posted on August 29, 2005 at 08:18

We have projects with RS232-communications from our hardware to PC. Now we create new hardware with STR710-processor and we would like to use USB insread of RS232. Is there an easy way, to modify the old software for this?

What have I to do, when I simply want to communicate from a PC to our hardware?

Many thanks for good answers!

info80
Associate II
Posted on August 29, 2005 at 10:27

Hi

I'm using uVision 3 from Keil with Keil-C-Compiler.

Regards

info80
Associate II
Posted on August 30, 2005 at 06:50

Hi,

I have ULINK and that is all ok. I'm speaking from the communication on target to PC. I have to write software for new hardware with STR710, that will communicate over integrated USB. I'm looking for software-examples to use USB.

Regards

thierry239955_stm1_st
Associate II
Posted on February 22, 2006 at 14:39

I have the same task as yours.

Did you get something ?

shangdawei1
Associate II
Posted on February 22, 2006 at 20:57

I have to write software for new hardware with STR710, that will communicate over integrated USB. I'm looking for software-examples to use USB.

Has anybody an example for Keil ARM ?

shangdawei1
Associate II
Posted on February 23, 2006 at 08:28

Quote:

On 23-02-2006 at 08:55, Anonymous wrote:

Hi,

If you are using Keil uVision3, you can find an example for USB in the install directory of Keil (Keil\ARM\Examples\STR71xLibUSB)

Rgds,

Zouhair

OK, i found an example for USB. Then i will make it as USB Bulk.

stephane23
Associate II
Posted on February 23, 2006 at 09:31

I’m in search of a same example but for ST evaluation board MB393B.

If possible an example that use a standard driver…

Thanks in advance,

Stéph.

stephane23
Associate II
Posted on February 23, 2006 at 12:57

I’m in search of a same example but for ST evaluation board MB393B.

If possible an example that use a standard driver…

Thanks in advance,

Stéph.