cancel
Showing results for 
Search instead for 
Did you mean: 

compiler

seeguard
Associate II
Posted on November 12, 2003 at 06:48

compiler

This discussion is locked. Please start a new topic to ask your question.
8 REPLIES 8
seeguard
Associate II
Posted on November 11, 2003 at 13:23

hello,

May someone tell me how can I define the Metroworks compiler

to compile ST7 (72F521) software package in LARGE mode.

(by default it's create a SMALL mode project)

thanks,

Atz :

sjo
Associate II
Posted on November 11, 2003 at 13:29

Have a look athe the -m compiler option in the docs.

-ml (large memory model) - this is the default if no option specified.

Regards

sjo
seeguard
Associate II
Posted on November 11, 2003 at 14:52

thanks,

I use the metroworks IDE. can you point me

where I can configure the the coimpiler switshes

as well as -ml ,optimization, ...... ?

atz

jatin
Associate II
Posted on November 12, 2003 at 02:26

You can configure the -ml option in the .env file.

seeguard
Associate II
seeguard
Associate II
Posted on November 12, 2003 at 05:08

I'm trying again.

please see the attached file.

atz

________________

Attachments :

hello_jatin.doc : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Gz&d=%2Fa%2F0X0000000bWT%2FSyl9cnAMeKFXYn86SDxz6PqOg891AaUibDWzZbI8Rws&asPdf=false
sjo
Associate II
Posted on November 12, 2003 at 05:58

The button next to drop down combo is the project settings.

In the settings panel select Compiler for ST7.

Select Options on the right, then the code generation tab.

Check Memory Model - selecting the required option.

Hope this helps

sjo
seeguard
Associate II
Posted on November 12, 2003 at 06:48

Thank you.

It's works!