2012-07-26 2:00 PM
Hi there,
I want a fifo buffer of all messages on the CAN bus in the order they arrived. This can include standard and extended IDs. At this stage I can not seem to get a message object to receive either a standard or extended ID. It always has to be one or the other! Any ideas if this is possible? #st10f276-can-can-c2012-07-26 3:05 PM
RESOLVED - Just need to make sure MXTD is clear. I did have this clear but had other issues... So the answer to my question is yes it is possible to receive standard and extended IDs in the same message object.