2025-07-27 9:56 AM - last edited on 2025-08-09 2:46 AM by Andrew Neil
hello people! thanks for coming to help me. I'm having problem in debugging a code which is written in bare metal programming. the concept of the program is that it uses the inbuilt led and temperature sensor. the led blinks according to the adc value of the temperature sensor. But the led is constantly on instead of blinking. i tried a simple led blinking code it worked fine but this temp code its making the led to be constantly ON I dont know what the problem is . i will give the code i wrote below plz help me
#include<stdint.h>
#include<stdio.h>
//registers used
volatile uint32_t *RCC_APB2ENR =(volatile uint32_t *)0x40021018;
volatile uint32_t *GPIOx_CRH =(volatile uint32_t *)0x40011004;
volatile uint32_t *GPIOx_ODR =(volatile uint32_t *)0x4001100C;
volatile uint32_t *ADC_SQR3 =(volatile uint32_t *)0x40012434;
volatile uint32_t *ADC_SMPR1 =(volatile uint32_t *)0x4001240C;
volatile uint32_t *ADC_CR2 =(volatile uint32_t *)0x40012408;
volatile uint32_t *ADC_SR =(volatile uint32_t *)0x40012400;
volatile uint32_t *ADC_DR =(volatile uint32_t *)0x4001244C;
void internal_tempsensorInit(){
*RCC_APB2ENR |= (1<<4);//PORTC clock enabled
*RCC_APB2ENR |= (1<<9);//ADC1 clock enabled
//port c pin 13 configuration
*GPIOx_CRH &= ~(0xF << 20); // Clear bits
*GPIOx_CRH |= (0x2 << 20); // 0b0010 = Output, 2MHz, push-pull
*ADC_SQR3 &=~(0x1F<<0);//clear SQ1
*ADC_SQR3 |=(16<<0);//select channel 16
*ADC_SMPR1 &=~(0x7<<18);//clear sample time for channel 16
*ADC_SMPR1 |=(0x7<<18);//set sample time (239.5cycles)
*ADC_CR2 |=(1<<23);//set temperature sensor
for (volatile uint32_t i = 0; i < 10000; i++); // ~short delay
*ADC_CR2 |=(1<<0);//set ADON ADC ON
//CALIBRATION
*ADC_CR2 |=(1<<3);//RESET calibration
while(*ADC_CR2&(1<<3)){//wait until its cleared
}
*ADC_CR2 |=(1<<2);//SET calibration
while(*ADC_CR2&(1<<2)){//wait until its cleared
}
//continuous conversion
*ADC_CR2 |=(1<<1);
}
uint16_t adcread(){
*ADC_CR2 |=(1<<22);//start of conversion
while(!(*ADC_SR&(1<<1))){
}
return (uint16_t) *ADC_DR;
}
static inline void delay_ms(uint32_t ms) {
// crude ~ms delay assuming ~72MHz, adjust if too fast/slow
for (uint32_t m=0; m<ms; m++) {
for (volatile uint32_t i=0; i<72000; i++) {
__asm__("nop");
}
}
}
int main(){
internal_tempsensorInit();
(void)adcread(); // throw away first reading
while (1) {
uint16_t analog_value = adcread();
float Vsense = (analog_value * 3.3f) / 4095.0f;
float temperature = ((1.43f - Vsense) / 0.0043f) + 25.0f;
uint32_t ms = (uint32_t)(temperature * 50.0f); // ~1.5s around 30°C
if (ms < 100) ms = 100; // clamp for visibility
if (ms > 2000) ms = 2000;
*GPIOx_ODR &=~ (1<<13);// LED ON (active-low)
delay_ms(1000);
*GPIOx_ODR |= (1<<13); // LED OFF
delay_ms(1000);
}
}Edited to apply source code formatting - please see How to insert source code for future reference.
2025-07-27 10:26 AM
Your programming style is for 5 months in Alcatraz...
And FYI code place here as code:
static inline void delay_ms(uint32_t ms) {
// crude ~ms delay assuming ~72MHz, adjust if too fast/slow
for (uint32_t m=0; m<ms; m++) {
for (volatile uint32_t i=0; i<72000; i++) {
__asm__("nop");
}
}
}is ecologic catastrophe.
Try debug your code !
2025-07-27 10:04 PM - edited 2025-07-27 10:06 PM
I have two comments: