2016-09-14 2:29 AM
I have used eDesign for a buck converter design approach (see attachment). However, I noticed that the suggested components value are not the same as the ones on
. What is the reason for the differences (especially at the compensation)?Thanks in advance for your support.2016-09-21 11:45 PM
Patrizia Bellitto
2016-09-22 12:43 AM
Hello,
I forwarded your question to the application engineer a week ago, I'll reply as soon as he gives me some feedback.Thanks for your interest and patience!2016-12-13 4:32 AM
Hello Patrizia,
Have you heard back from your application engineer? I have been waiting a long time for this feedback.
Thanks for your understanding!
2016-12-14 2:00 AM
Hello,
sorry, you are right...Could you tell me exactly the specification of your application?
Because the application note you pointed out expects two outputs, while eDesign allows only one.
Thanks
Patrizia
2016-12-14 2:21 AM
Hi,
Yes, the one that I pointed out has 2 outputs but it should make a big difference on the design as for the 5V output a linear regulator is used. So, my understanding is that I should have a similar design (on eDesign) if I would use the same specification as STEVAL-ISA116V1 for the 16V.
I am looking forward to hearing from you.
Regards,
2016-12-14 5:43 AM
Hi, I verified the components suggested by the application note and there are a lot of differences between them and what suggested by eDesign. Not always there is a correspondence because application note applies to a particular situation while eDesign must provide a general optimized solution. You can try to modify your design so that it is more similar to the BOM in AN4562, in terms of inductor, output capacitor, bandwidth: however, consider that in the next days, I hope tomorrow, we are publishing a new release where the compensation net for these designs is further optimized. I'll let you know when it will be online.
2016-12-19 8:43 AM
Hello, just to inform you that the latest release of eDesignSuite contains an optimized compensation net for VIPer buck solutions.
Regards,
Patrizia