cancel
Showing results for 
Search instead for 
Did you mean: 

[ANN] eLua (Lua for microcontrollers) 0.6 released

darkore
Associate II
Posted on October 08, 2009 at 19:09

[ANN] eLua (Lua for microcontrollers) 0.6 released

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
darkore
Associate II
Posted on May 17, 2011 at 09:59

eLua is an effort to expand the presence of the Lua programming language in the embedded world (MCUs). It is meant to be a complete MCU development environment. It currently runs on a number of ARM variants, as well as Cortex, AVR32 (and i386 as a proof of concept). Version 0.6 was released, this is the changelog:

* License changed to MIT

* Web page and documentation completely redesigned

* Documentation available offline

* Added documentation in portuguese

* Added support for AVR32 CPUs

* Added support for STM32 Cortex-M3 CPUs

* Added ADC module with support for moving average filters

* Added support for multiple toolchains

* Added an ls (or dir) shell command

* Added new examples: pong, tetrives, spaceship (games), logo (graphics), adcpoll, adcscope (ADC operations)

* Added the LTR (Lua Tiny RAM) patch

* ROM FS content can be specified per board now

* API semantic revisions (old code might not be compatible)

You can find all the project documentation at

http://www.eluaproject.net

Thanks,

Bogdan