Skip to main content
sjo
Associate III
September 23, 2004
Question

ADC - str7 library

  • September 23, 2004
  • 2 replies
  • 756 views
Posted on September 23, 2004 at 12:04

ADC - str7 library

This topic has been closed for replies.

2 replies

sjo
sjoAuthor
Associate III
September 23, 2004
Posted on September 23, 2004 at 09:26

STR7 Gurus,

Another query regarding the str7lib

The adc lib function uses the formula:

PRESCALER = APB2_FREQ / (SAMPLE_FREQ * 512 * 4)

to calculate the prescaler.

The datasheet states that the result from the above formula must be halved

APB2_FREQ = 16MHz

SAMPLE_FREQ= 500Hz

PRESCALER= 16M/(500*512*4)

PRESCALER= 16

according to datasheet (page371 v3.0) the precaling factor must be 8 to obtain a prescaler of 16.

which is correct ?

So far I have been very impressed with the str7, but I must put my comments regarding the adc - its really bad.

I have just realised all conversions require calibrating for offset/gain errors, after just spending a few hours diagnosing really strange conversion results.

Are there any good tips on the adc for the str7?

Regards

sjo
hichem2
Associate
September 23, 2004
Posted on September 23, 2004 at 12:04

Hi, sjo

I agree with you concerning your remark;

The result mentioned in the datasheet is the correct one and the formula used in the ADC lib to compute the prescaler must be replaced by the following one:

PRESCALER = APB2_FREQ / (SAMPLE_FREQ * 512 * 8) .

Best Regards

Hich

[ This message was edited by: Hich on 23-09-2004 15:44 ]

[ This message was edited by: Hich on 23-09-2004 15:45 ]