2008-03-12 3:49 AM
2008-03-12 3:49 AM
I use 6 channel in scan mode and I setup them in this way (MCLK is 36 MHz)
Code:
static void initAd(void)
{ GPIO_InitTypeDef GPIOx_InitStructure; ADC_InitTypeDef ADC_InitStructure; /*-----------------------------------GPIO3 ----------------------------------*/ /* GPIO3 Clock Enable */ CFG_PeripheralClockConfig(CFG_CLK_GPIO3, ENABLE); /* GPIO3 Configuration */ GPIOx_InitStructure.GPIO_Mode = GPIO_Mode_HI_AIN_TRI; GPIOx_InitStructure.GPIO_Pins = GPIO_PIN_4 | // AIN0 GPIO_PIN_5 | // AIN1 GPIO_PIN_6 | // AIN2 GPIO_PIN_7 | // AIN3 GPIO_PIN_8 | // AIN4 GPIO_PIN_9; // AIN5 GPIO_Init (GPIO3, &GPIOx_InitStructure); /*---------------------------------ADC---------------------------------------*/ /* ADC Clock Enable */ CFG_PeripheralClockConfig(CFG_CLK_ADC, ENABLE); /* ADC Configuration */ ADC_StructInit(&ADC_InitStructure); ADC_InitStructure.ADC_Calibration = ADC_Calibration_OFF; ADC_InitStructure.ADC_AutoClockOff = ADC_AutoClockOff_Disable ; ADC_InitStructure.ADC_ConversionMode = ADC_ConversionMode_Scan ; ADC_InitStructure.ADC_SamplingPrescaler = 0x7; // Inutile ma 36/14=2.571 MHz ADC_InitStructure.ADC_ConversionPrescaler = 0x7; // 36/14 = 2.571 MHz // sampling time 11.33 us (1 ch); 70 us (6 ch) ADC_InitStructure.ADC_FirstChannel = ADC_CHANNEL0 ; ADC_InitStructure.ADC_ChannelNumber = 6; ADC_Init(&ADC_InitStructure); /* EOC interrupt Enable */ EIC_IRQChannelConfig( ADC_IRQChannel , ENABLE ); EIC_IRQChannelPriorityConfig( ADC_IRQChannel, 1); ADC_ITConfig(ADC_IT_ECH , ENABLE); /* Enable ADC */ ADC_Cmd(ENABLE); }The interrupt handler is something like thisCode:
void ADC_IRQHandler(void); void ADC_IRQHandler(void) { if(ADC->PBR == 0) { while(1) GPIO0->PD ^= 16; // output a signal } /* Clear ECH Interrupt pending bit */ ADC_FlagClear (ADC->PBR); // some stuff } with my oscilloscope I can see that after a while the program loops in while(1). It seems that is raised an interrupt without any panding bit set. Is it possible? Is the adc well configured? What is wrong with code I wrote? thanks