2008-03-07 4:58 AM
2008-03-06 6:08 PM
Hi
I use STR710. When I use 48Mhz(Main Clock) with EMI_WAITSTATE(10), muc works very well. But I changed Main clock to 32Mhz, also EMI_WAITSTATE(10), but MCU could not boot even if we change form CS0 to CS3. How can I find EMI_WAITSTATE value ? Is there any formula ? Thank you2008-03-06 6:53 PM
It depends on MCLK. If you low the clock on a 25%, I suppose you should increment the wait state in a 25%, so I'll consider a value of 13.
However, you'll get the best value though a trial-error procedure :-]2008-03-07 4:58 AM
Quote:
you'll get the best value though a trial-error procedure :-]
Even better, consult the timing sections of the datasheets involved. And use an oscilloscope to verify that the required access cycle timings are satisfied.