2007-04-26 2:26 AM
2007-04-24 3:51 AM
Hi all,
is it possible to activate the input voltage amplifier for just one single ADC input ? For eg: AIN0 range 0-430mV ( 5VDD ) and the rest of AINx range 0-5V ? BR Tomasf2007-04-24 4:14 AM
Tomas,
As described in fig 49 of the datasheet, you can see that there is only one amplifier which is connected to the Analog multiplexer output. So you must enable the amplifier thanks to the AMPSEL and configure correctly the fADC (below 2MHz) thanks to bit SPEED and SLOW before selecting the channel you want to convert. By changing the AD channel you will automatically launch a new conversion. Hoping you will be successful with your application. Best regards Laurent2007-04-24 8:09 PM
Hi Laurent,
thanks for your fast reply. Ok - so all or nothing. Pity. I just needed one single ADC input in ''13-bit mode'' the rest in ''10-bit mode'' for a new application. Take care, Tomas2007-04-25 4:54 AM
Tomas,
You can manage this by software. It is a little bit more complex but not so much ! Take care too. Laurent2007-04-25 7:51 PM
Hi Laurent,
Aha - I am not so skilled to figure it out. Is it possibly so that you are able to assist me ? Take care, Tomas2007-04-26 2:26 AM
Hi,
For more information you can refer to AN1830. And if you have still issue don't hesitate to ask questions in the forum. Best regards Laurent