2005-06-18 10:44 PM
µPSD 3334-DV : Clock signal on an output pin ?
2011-05-17 3:07 AM
Hi,
I work with the µPSD 3334-DV. I would like to know if it is possible to make a clock signal as an output. For example, I would be pleased to make as an output the signal PCA0CLK Thank You very much for the answer I will catch on that forum. Alexis2011-05-17 3:07 AM
hi,
you cannot directly route PCA#CLK to an output. but you can use the TCM# to i.e. toggle a pin according to PCA#CLK. if you really need a ''fast'' clock-output, you can route the _ale-signal to an output-pin in the PLD. (but then you should not use idle-mode/power-down-mode/reduced-frequency-mode, because this also stops/reduces the _ale.)