2017-10-26 01:37 AM
The output Voltage expected is 6V and output is constant for 110VAC input. But the output is turning ON/OFF for 220V input. Please let me know to resolve this issue. I have followed the ST Design suite for the design.
#viper16ld #viper162017-10-30 02:23 AM
Hello,
could you please provide the complete specifications?
You speak about a 6V output voltage, but in the schematic the expected value is 5V, and even the output divider is sized for this last value.
Regards,
Patrizia
2017-10-30 08:14 PM
Complete Spec is Non Isolated Buck Topology with Universal mains 85-265VAC, Expected Output is 5V with 5% voltage regulation.
I have increased to 6V Since there is drop of around 1V from No load to full load voltage.
As I said the Output @ 110V was steady but @ 220V, voltage was fluctuating as shown in picture.
2017-11-02 03:10 AM
Hello,
we need even the output current, please.
Regards