2016-06-01 05:58 AM
Hello,
I've a problem using the Viper06L Spice Model in Orcad 16.6 Lite. If I start the simulation I get the following error:ERROR(ORPSIM-15113): Model DZener used by X_U1.X_VIP06_CTRL_A1.X_X_OLF.D_D5 is undefinedYes I downloaded the newest model from eDesign Studio and I've just updated my Orcad.Any ideas?2016-06-06 03:14 AM
Hello Jens,
the Orcad model contained in eDesign is not updated to the latest version. It is better if you download the most recent release from the VIPer06 product page, at this link: We'll remove the old model from eDesign in the next release. Thanks a lot for your reporting. Best regards, Patrizia BellittoeDesignSuite developers team2016-06-07 05:37 AM
Hello Patrizia,
I tried the model you linked but I still get the same error message.2016-06-07 06:03 AM
Have you downloaded version 2.0? It is a zip containing the model for all the three part numbers (VIPer06X/L/H)
2016-06-08 02:29 AM
Hmm. Ok I didn't see this. But now I tried V2.0 and I get a different error:
ERROR(ORPSIM-15113): Model Q40235 used by X_U1.X_VIP06_CTRL_A1.Q_Q2 is undefined2016-06-08 03:42 AM
Actually I'm going crazy with this model. Now I got it working with model for Q40235 from http://robustdesignconcepts.com/files/pspice/pmindex.htm --> bipolar.lib
But the problem is the Viper don't start switching. I'm not new to Spice Tools but I've no idea what's the reason for that.2016-06-08 05:11 AM
Hello Jens,
I'm sorry for the problems you are experiencing with this model.Althoughyou already solved the previous issue, I'm sending in attachment a new version of the model that contains the missing bipolar library. Regarding your last post, please be sure that you set the option ''initialize al FF to 0'' as described in the short document attached to the model. If you have already done it, Ineed the complete OrCAD project you are trying to simulate to help you.Would it possible to haveit? Thanks for your patience. Best Regards, CarmeloVicariFrom: koehler.jens
Posted: Wednesday, June 08, 2016 12:42 PM Subject: Orcad and Viper06L ModelActually I'm going crazy with this model. Now I got it working with model for Q40235 fromhttp://robustdesignconcepts.com/files/pspice/pmindex.htm -->bipolar.lib
But the problem is the Viper don't start switching. I'm not new to Spice Tools but I've no idea what's the reason for that. ________________ Attachments : VIPER06.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzEE&d=%2Fa%2F0X0000000bIe%2FQIb18IuTnzdCPWUYqdqIl4l6QEy5p9EQw5VGWmwoTzc&asPdf=false2016-06-09 11:03 PM
Hello,
I'm not able to open the attached zip file. It seems to be defective. I already set initialize FFs to 0 so I send you my project. Attached you'll find my test project. Hope it helps. ________________ Attachments : Test_Viper.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006HzE4&d=%2Fa%2F0X0000000bId%2FFzsztaLBV3fUZoDSaTC3InHb7Wm43C12BbdsmCsguNM&asPdf=false2016-06-10 12:34 AM
Dear Jens,
the VIPER06 model did not start switching because it needs a rising edge on the DRAIN PIN to detect the power on. Toreproduce this behaviorI just replaced the VDC source with a VPULSE sourcewhich goes from 0V to 350V. In addition, the coupling modelKBREAK was not working properly. I replaced it with the K_Linear device from the analog library of ORCAD. I'm sending in attachment the updated project. Inside the ''en.VIPER06_spice'' folderyou can also findthe latest version of the VIPER06 model, the same thatyou were unable to open from my previous post. Hope it doesn't get corrupted again. Feel free to contact me for further clarifications. Best Regards, Carmelo ________________ Attachments : Test_Viper_v2.0.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006Hz2V&d=%2Fa%2F0X0000000bIc%2FWWTEIMV.nMJdV26nW4fcubKh68.dzj8dYHd703_8ppo&asPdf=false