2018-05-14 05:20 AM
I've just used EDesignSuite to design a Flyback PSU based around a L6566B
As part of this, it has designed me a transformer, in around half a page of small, poorly formatted, dense, closely type text.How do I export this text so as to send it off to be made? It does not seem to be possible to get it out in any useful form?(Printed page is NOT 'useful' in this context)Surely you do not expect me to slowly, tediously and laboriously re-type all this text, probably introducing expensive errors as I go?#transformer-export-design-as-text2018-05-14 05:30 AM
Hello Andrew,
have you already tried to print the design report?
Opening the print view you can save it as PDF, otherwise you can copy the text and paste wherever you want.
Best regards,
Patrizia
2018-05-14 05:57 AM
Sorry it is not working on Linux, on Windows I can copy/paste without problems.
In next release we can expand the XML BOM you can save from the menu Save -> Export BOM as XML..., so that all the transformer information are given as text format.
Regards,
Patrizia
2018-05-14 07:35 AM
The PDF is a graphic, which I cannot copy and paste from, I can't even select any text.
I tried selecting the text and copying pasting, I can select it, but when I paste I just get blank text, wherever I try and copy it from.2018-05-14 07:40 AM
This is what I have just copied directly from the print view:
Transformer Design:
Core: Type EE16S - Area Product 718 mm^4 - Orientation Vertical Volume (Ve) 795 mm^3 - Cross-Sectional Area (Ae) 21.70 mm^2 - Bobbin Winding Area (Aw) 33.10 mm^2 Bobbin Average Turn Lenght 37.10 mm - Bobbin Centr. Leg Lenght 8.70 mm Core Gap: 0.24 mm expected Inductance factor (AL): 118 nH/N^2 expected Primary: Turns 233 - Layers 18 - Paralleled wires 3 Wire: Manufacturer Wurth Elektronik - Part Number PN180 9283-0038 - Type Single Number of strands 1 - Strand copper Ø 0.102 mm - Wire gross Ø 0.112 mm Resistance per meter 2.2372 Ω/m Secondary: Turns 9 - Layers 3 - Paralleled wires 3 Wire: Type Solid_G2 - Number of strands 1 - Strand copper Ø 0.425 mm Wire gross Ø 0.488 mm - Resistance per meter 0.1244 Ω/m Auxiliary: Turns 20 Wire: Type Solid_G2 - Number of strands 1 - Strand copper Ø 0.100 mm Wire gross Ø 0.125 mm - Resistance per meter 2.3330 Ω/mIf you export the project as PDF, you can send directly that file to the transformer manufacturer, in the report there is all the necessary information.
2018-05-14 07:46 AM
It really is not working here - (Chrome / Linux).
The PDF form is not very useful for me, for a number of reasons it really does need to be text.I have a typist retyping it now, as I cannot wait.2018-05-16 01:34 AM
Hi Andrew,
just to inform you that in the new release a more complete report on the transformer design is exported when you save the project as XML file, that you can easily open as Excel table.
Best regards,
Patrizia
2018-05-16 03:40 AM
Thanks. When does the new release come out?
I've also been looking at some of the AC/DC isolated converters in eDesign.
Some of them allow you start a design, but are then incapable of
producing a design that meets the thermal ratings of the main chip, and
not by a bit, by a lot.
Some of them produce a design which is so lacking in information about
the output sense and opto as to be useless. They give so little
information or reference that you effectively need to start the design
yourself.
Are these problems known about and being addressed?
A.
2018-05-16 03:47 AM
The new release was published yesterday.
Do you mean designs with VIPer devices?
2018-05-16 03:51 AM
Yes. There seem to be a lot of problems with them. I am using one based
on VIPer37HD. I need euro mains (185V to 265V AC) input and isolated 15V
@1.2A amps. The process was 'very frustrating'. It's for a high volume
consumer product and I need to be very cautious.
A.