2008-04-25 05:36 AM
2008-04-25 02:22 AM
Hello,
I'm trying to initializate a vs6724 camera and i don't figer it out, i've wrote an email to tehnical suport section and they answare me that the informations for this camera are no longer available.Have anyone succeded working with this camera? I'm not finding anything on the internet. I'm just writeing and reading to the hardware registers, and when it comes about the user registers,i can write them, but when i read them with the read I2C function, it is returning oxooh each time(the I2C functions are right 100%, they are working for the hardware registers). Thank you!2008-04-25 05:36 AM