2014-11-02 06:35 PM
Hi all,
I encountered few issues when using STVP to program a ST7Flites5. Can anyone advice me on possible solutions? Tks in advance. 1. STVP does not provide a erase before programming option for ST7Flites5. This particular programming job specify its option byte with a read protection on and after programming on STVP, I could not do any programming or verification again, cos it keep saying it is protected. However, ST7_PGM is able to do that (it erase and program), just that it only accept hex data file but no srec. 2. Though I could program and verify in STVP using its graphical interface, the STVP_cmdline could not connect to the ST7Flites5. Please help!? BTW, I am only doing programming on the ST7 and frankly, I know very little about the uC. So your patience is needed here. :-) #st7-stvp-stvp_cmdline2014-11-03 05:31 AM
Hello,
1) Simply remove the Protection by reprogramming option byte with Read-out protection OFF. That will erase all the Program memory. If you use STVP in Project mode, you can have an option to do that automatically: ''Unlock protection before a programming cycle''. It will take default option byte value (with protection OFF) and program the device. 2) What is the error you get (error.log or result.log) ? Maybe the arguments are wrong (syntax error?). If you specify the same arguments as you did with STVP gui, it must work. Example: STVP_CmdLine.exe -Port=USB -BoardName=RLINK -Device=ST7FLITES2/S5 -ProgMode=''ICP OPT Disable'' -FileProg=test_LiteS5.s19 -FileOption=OPTIONS_ROP_ON_LiteS5.s19 If the device is protected, you must use the GUI interface to save an option byte file with ''Read-out protection OFF'' and program the option first via STVP_CmdLine. STVP_CmdLine.exe -Port=USB -BoardName=RLINK -Device=ST7FLITES2/S5 -ProgMode=''ICP OPT Disable'' -FileOption=OPTIONS_ROP_OFF_LiteS5.s19 Laurent2015-06-17 04:49 PM