2009-07-30 08:20 AM
2011-05-17 12:59 AM
Hello Gents and Ladies
I recently bought this module and been playing with it for a little. According to SCM-STR912CS-A1-1a.pdf the can transceiver already has a 120ohm terminating resistance for the can driver. Is there any way to disable this resistance since i want to use the module to listen to a can network that already has both terminating resistances. If not what are my options? Can i use an external can transceiver and transfer the functionality of the Can Rx and Can Tx to other pins. This module is already limited with 12 I/O's Any help will be appreciated. My Best Regards-