2020-12-03 11:36 PM
2020-12-04 4:11 AM
As I already wrote: unfortunately we cannot propose any device fulfilling your requirements.
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2020-12-04 1:34 AM
I'm really sorry, but unfortunately there is no direct replacement available.
Maybe we could suggest an alternative if you provide the required parameters and/or the circuit currently used?
Regards
/Peter
2020-12-04 1:41 AM
Thanks for your reply.
Here is my requirement:
PWM dimming frequency is 10KHz and switching frequency is 250KHz or better.
Please suggest with the suitable IC.
2020-12-04 1:45 AM
Since it is an LED driver, the desired input voltage range, the LED string voltage and the LED current are missing?
/Peter
2020-12-04 1:50 AM
2020-12-04 2:13 AM
2020-12-04 2:52 AM
Unfortunately we cannot propose a device fulfilling of your requirements.
The closest device is the STLD40D, but its input voltage range is 3...5.5V and its maximum peak current is probably insufficient for an LED current of 100 mA when fed by 3 V.
Good luck!
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2020-12-04 3:42 AM
Sir, This STLD40D IC can capable of 10LED's in series only. Can you suggest any other IC for my requirement of 44LED's.
2020-12-04 4:11 AM
As I already wrote: unfortunately we cannot propose any device fulfilling your requirements.
When your question is answered, please close this topic by choosing Select as Best.
/Peter
2021-06-28 10:33 AM
This is VERY inconvenient for STMicroelectronics to just discontinue a product and offer no alternate. And..."sorry, we just don't have a device that fulfills your requirements"... is the best you can do?