cancel
Showing results for 
Search instead for 
Did you mean: 

ST10F276 ALE length DeMuxed Bus

urik
Associate II
Posted on March 07, 2006 at 04:48

ST10F276 ALE length DeMuxed Bus

3 REPLIES 3
urik
Associate II
Posted on March 05, 2006 at 02:10

Hello,

if i use the EBC in DeMuxed bus in 64 MHZ can i choose the ALECTL to be 0 -> this causes (according to the data sheet) the time of t5(ALE High time) to be -1.5ns approx?

is that leagal? i want to do this to achive the max out of the part.

thanks,

Uri.

urik
Associate II
Posted on March 06, 2006 at 06:19

Hello,

if i want to squize the max performance out of the ST10F276 and i use the Demuxed bus, this time is of no importance to me, can i use the ALECTL = 0 ?

or that will cause the device to malfunction?

Regards,

Uri.

urik
Associate II
Posted on March 07, 2006 at 04:48

Thanks.