2006-03-09 03:34 AM
So the Atlas is the only STPC that will sirvive?
2006-03-08 10:36 AM
Hi,
I received the end-of-life notice for the STPC processors. It says that all STPCs are EOLed, but the Atlas is not in the list. Is it a typo, or is the Atlas going to survive longer than another year? Curiously the ST rep did not answer back my question. What is the official word about the Atlas? The sales of Atlas might rise, because it looks like it is going to be the only remaining part on the planet to support the ISA bus. Geode disappears, Via Eden will go, STPCs go. Shame! Felix2006-03-09 03:34 AM
Yes, Exactly all STPCs are EOLed :-( but the STPC Atlas is kept. For the moment, I don't have an exact date wut what is sure that it will survive more than one year.