cancel
Showing results for 
Search instead for 
Did you mean: 

Scatter file and DFU application

andrea239955_st
Associate
Posted on May 18, 2007 at 11:22

Scatter file and DFU application

1 REPLY 1
andrea239955_st
Associate
Posted on May 18, 2007 at 11:22

Hi guys,

I have problems using the DFU USB feature. :(

The first one is that I have been able to compile and download the example only with the IAR toolchain. I first tried with RVDK. I had to create the project by myself. I compile without error, but the RVDG is not able to downlaod the image axf created (= RVDB gets stuck). Maybe it is just a matter of project setting...

The second (and the main) is:

[B]how does my scatter file should look like \B] to buil images that can be downloaded via USB? I tried just modifing the one I used to have. I attached the scatter file here for reference.

I got the following error message.:

rmlink: Error L6202: __main.o(!!!main) cannot be assigned to non-root region 'FLASH'

armlink: Error L6202: anon$$obj.o(Region$$Table) cannot be assigned to non-root region 'FLASH'

I would really appreciate if someone can help me on that. Can you please post a scatter file? I have not been able to find any specific documentation (even in the USB dev kit package).

Thank you very much.

Andrea