2024-03-22 02:57 AM - edited 2024-03-22 02:59 AM
Hi
In our design, we incorporated the IMS T225-F20E component. This part necessitates a clock with a frequency of 5 MHz. According to note 3 in the attached image, crystal oscillators with a 200 ppm (parts per million) tolerance can be employed. However, this information pertains to scenarios where two devices are connected together by a link.
Now, the question is: What is the allowable tolerance for the clock oscillator if only one device is used?”
I am currently working on crystal aging analysis. It would be beneficial if you could furnish the allowable tolerance data for the device.
Thanks in advance
Solved! Go to Solution.
2024-03-22 01:00 PM
Well, this is a question about a device that was obsoleted decades ago and about which ST no longer has any information. However, I can still remember the parts a little.
When using the transputer as a single device, the absolute tolerance of CLKIN is quite irrelevant, the timing of the edges is more important. This is also evident from the lack of min and max values for CLKIN Period.
Hope this helps a bit?
Regard
/Peter
2024-03-22 01:00 PM
Well, this is a question about a device that was obsoleted decades ago and about which ST no longer has any information. However, I can still remember the parts a little.
When using the transputer as a single device, the absolute tolerance of CLKIN is quite irrelevant, the timing of the edges is more important. This is also evident from the lack of min and max values for CLKIN Period.
Hope this helps a bit?
Regard
/Peter