Skip to main content
robosoft
Associate III
January 25, 2008
Question

Redirect stdout in C++

  • January 25, 2008
  • 3 replies
  • 1030 views
Posted on January 25, 2008 at 03:43

Redirect stdout in C++

This topic has been closed for replies.

3 replies

robosoft
robosoftAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:49

Thanks for response !

I think its better to write my own printf function.

Luc

mark9
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:49

You should not modify the struct. To redirect stdout (or stdin, stderr) the standard way is

console = freopen(''\MYLOGFILE.TXT'',''r+'',stdout); // ''r+'' means read/write

assuming you have already written the low level drivers for your file system or IO stream.

robosoft
robosoftAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:49

Hi,

I use the KEIL Realview MDK-ARM

I want to define a functionpointer in the __FILE struct (stdio.h).

By changing this functionpointer in my mainprogram I can redirect stdout to some device.

To do this I changed the file retarget.c to following

 

#include

 

 

extern ''C'' {

 

struct __FILE {

 

int handle;

 

int *(*stdoutProc)(int ch); //THIS IS THE FUNCTIONPOINTER I CREATED

 

};

 

 

FILE __stdout;

 

FILE __stdin;

 

 

 

InitStdOut(int *MyStdOut(int Ch)) {

 

__stdout.stdoutProc = MyStdOut;

 

}

 

 

int fputc (int ch, FILE *f) {

 

__stdout.stdoutProc(ch);

 

return(ch);

 

}

 

} //extern C

 

I did not test the code, so maybe the code doesn't do the thing I want to do, but however I can compile it without errors !

When I rename all the files to *.cpp, to use the compilers C++ extentions, I have the error (at the line FILE __stdout;)

error #70: incomplete type is not allowed

How can I add a functionpointer to the __FILE struct in C++ environment ????

Thank you !