2008-05-28 12:19 PM
Question about the design of JTAG interface
2011-05-17 02:32 AM
Hi,
I am designing a system based on STR91* Microcontroller. Here I have one question about the design of JTAG interface. In the schematic of STR91* eval-board, there are two resistor which marked as ''10K_n.b.'' for the JTAG connector. When I checked the eval-board, there is no such resistor layout and they are just open. Is anybody can tell me what's the ''10K_n.b.'' represents? What these resistors are for?