2003-08-05 10:10 PM
Programming/Erasing the internal Flash of 269
2003-08-05 10:10 PM
I'm using AN 1496 wich is confusing. Trying to erase the chip as it was described in table 1 don't work. I load the program in the internal ram and than I want to erase the whole chip. The Watchdog was turned on, because of the running program before. Is this a problem? Of course I have to service the watchdog also during erasing or programming the flash. I need correctly running program-samples in assembler whow erasing and programming is done, not like the confusing AN. Please help me.