2005-08-24 12:34 AM
2005-08-23 10:48 PM
Thank for all the informations! You are very helpfully!
I attach all you have request to me in a .txt file in this message. Bye. ________________ Attachments : main.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0Ai&d=%2Fa%2F0X0000000bVE%2F6gI7r6VGbHbIm3haqHQ5tDvrs8WDmxRsts3XxjwXaE4&asPdf=false2005-08-23 10:52 PM
Excuse me. I have posted the wrong text file!
Now I post the correct version. Thanks ________________ Attachments : main.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0CY&d=%2Fa%2F0X0000000bVG%2Fk506rHjft8ppStRfFEVueAi6Zm6j1Ll3fwGsJmpW.PM&asPdf=false2005-08-23 10:55 PM
Excuse me but I have some problems with my browser!
I hope this is the correct version! Bye. ________________ Attachments : prog.txt : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0CT&d=%2Fa%2F0X0000000bVD%2FYLF4JT1rPYNI6moTKpPHRirm0rvLI6B6lZ.C7H5r4eY&asPdf=false2005-08-23 11:55 PM
Hi,
now I hope I've got it: You can use the option -Cni (no integral promotion on characters) to avoid promotion of characters to integrals. Please note that there seams to be a fault in the manual regarding the two char multiplication with -Cni. To get the option above please follow the way: Edit & ''project'' Settings [Alt+F7] & Compiler for ST7 and then select Options & Optimizations & [x] no integral promotion on characters That would suppress _CMPS. But I think you agree - the result is the same? Ciao WoRo2005-08-24 12:34 AM
You are my salvation!
Now all works correctly. Thanks. See you.