2009-02-10 12:03 AM
MEMS accelerometer with data logging software queries
2009-02-10 12:03 AM
Hi,
I have the EK302DL evaluation board that uses the LIS302Dl accelerometer. I wish to use this board with data logging software, to basically take values of the X, Y and Z accelerometer output registers and store them at 10Hz or 1Hz frequency. I can use the data logger software to send the commands *Zoff and *start to the accelerometer board, but the board will still not allow data to flow from it into the data logger software. Are there any reasons for this, is there anything else I can try? Can anyone help me with his? I would be very grateful! Thank you [ This message was edited by: t_ennis9 on 02-03-2009 12:34 ]