2004-01-11 11:43 PM
How to reliably identify the STPC Atlas (cpuid)
2004-01-11 09:46 PM
STPC lacks the cpuid instruction (available in Pentium and forward)
Is there an other way to identify it? I have to be able to determine if it is a STPC or an other 486 based processor (intel). Of cause I can try to identify it by reading data from ports that does not exist on the 486 like USB - but then we run into the same problem when we change processor the next time... /RogerL2004-01-11 11:43 PM
Found it.
Register DIR0 (DEVID) Described in ''Standard 486 Processor Core Programming Manual'' Chapter ''4.4.4.4 Configuration Registers''