2005-08-23 05:25 PM
How to do supplying the external battery power to sram in using upsd3254?
2011-05-17 03:08 AM
Now I meet with an important question in upsd3254, I want to supply external power to internal sram, not using the internal power supplying to internal sram,even if the chip power is still on.How can I do it? Any ideas are helpful,Thanks :-[
:-[2011-05-17 03:08 AM
hello,
you must define PC2 pin of UPSD in PsdSoft as sram standby voltage input,then connect this pin to battery backup circuits. ;-)