cancel
Showing results for 
Search instead for 
Did you mean: 

HDLC support

tim11
Associate II
Posted on January 10, 2006 at 14:56

HDLC support

3 REPLIES 3
tim11
Associate II
Posted on January 06, 2006 at 15:58

I have searched high and low and have not found any libraries for any of the development systems in support HDLC. Matter in fact, ST lists HDLC in all flyers and brochures and has an HDLC section in the reference manual but it is the only peripheral not supported by the STR7 standard library.

Are there problems with the HDLC function? The clocking options are quite limited with only one external clock input. There should have been atleast one clock I/O per RX and TX.

[ This message was edited by: tim35ca on 06-01-2006 20:30 ]

hichem2
Associate II
Posted on January 09, 2006 at 06:23

Hello,

Yes you are right, the HDLC library and user manual are not included with the standard STR71x software lib.

All the needed documentation and functions are already developed and wait for publication.

By the way all the asked info will be available on the web page as soon as possible.

With best regards,

Hich

;)

tim11
Associate II
Posted on January 10, 2006 at 14:56

Hich,

Thanks for the info. What timeframe are we looking at for ''as soon as possible''?

Cheers!

Tim