2005-11-16 09:14 PM
HDLC and ethernet with STR710
The goal is to use the HDLC port for an ethernet connection. Is it possible to do so ? if yes, which components to add between the STR710 and the RJ45 connector.