cancel
Showing results for 
Search instead for 
Did you mean: 

Getting last ST6 tools (AST6,LST6,WGDB6)

benoit239955
Associate
Posted on January 10, 2004 at 03:50

Getting last ST6 tools (AST6,LST6,WGDB6)

3 REPLIES 3
benoit239955
Associate
Posted on January 09, 2004 at 10:06

I reseved a start kit that i bought. The software on the CD ROM is not the last release.

Can you help to find a way to download the last version of AST6, LST6 and WGDB6 tools ?

Thanks.
sjo
Associate II
Posted on January 09, 2004 at 12:25

I can upload them if ST do not help, you can use the Raisonance toolchain with the starter kit aswell - its a much better tool to use.

These are the latest versions I have:

AST6 - v4.50

LST6 - v3.40

WGDB6 - v2.8.0

Regards

sjo
vikas2
Associate II
Posted on January 10, 2004 at 03:50

The CD-ROM you got may have the previous versions of AST6,LST6 and WGDB6. Find attached the latest versions for AST6/LST6 and WGDB6(2.8.0).

These packages are no more available on the ST site because these are not supported now and has been replaced by the Raisonance tool chain.

Like sjo, i will also suggest you to use Raisonance toolchain. Its better tool as it features a powerful macro-assembler, a linker, a C compiler and a state-of-the-art simulator and debugger. Its fully compatible with sources developped using the STMicroelectronics toolchain. Moreover, it supports all ST6 emulators: ST6xx-HDS2, Softec and CEIBO emulators. It is freely available(with only limitation of code size while writing code in C language) at www.stmcu.com/familiesdocs-html under Software Release section.

________________

Attachments :

ST6_Toolchain.zip : https://st--c.eu10.content.force.com/sfc/dist/version/download/?oid=00Db0000000YtG6&ids=0680X000006I0K3&d=%2Fa%2F0X0000000bXI%2FYESUKHjES7puHGkV.yHXuIJNmM0qSTpES93kSWXBonA&asPdf=false