Skip to main content
satnam
Associate III
July 2, 2009
Question

external interrupt 2

  • July 2, 2009
  • 3 replies
  • 1005 views
Posted on July 02, 2009 at 02:46

external interrupt 2

This topic has been closed for replies.

3 replies

satnam
satnamAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:58

Dear All,

I am trying to get external interrupt 2 on port pin 3.2 of MCU. I have done the following configuration but the code never enters the ISR section.

Also i have checked the configuration in simulator of KEIL, the VIC section shows that the group2 interrupt has been set, while i had set the extint2.

Please check the code and help me out with this problem.

/* Enable the GPIO3 */

SCU_APBPeriphClockConfig(__GPIO3, ENABLE);

SCU_APBPeriphReset(__GPIO3,DISABLE); /*out of RESET state*/

/* Enable WIU clock */

SCU_APBPeriphClockConfig(__WIU, ENABLE);

/* Enable VIC clock */

SCU_AHBPeriphClockConfig(__VIC,ENABLE);

SCU_AHBPeriphReset(__VIC,DISABLE); /* out of RESET state*/

// 3.2

GPIO_InitStructure.GPIO_Pin = GPIO_Pin_2 ;//

GPIO_InitStructure.GPIO_Direction = GPIO_PinInput;

GPIO_InitStructure.GPIO_Type = GPIO_Type_OpenCollector;

GPIO_Init (GPIO3, &GPIO_InitStructure);

VIC_Config(EXTIT2_ITLine, VIC_IRQ,2);

VIC_ITCmd(EXTIT2_ITLine, ENABLE);

WIU_DeInit();

WIU_StructInit(&WIU_InitStruct);

WIU_InitStruct.WIU_TriggerEdge = WIU_FallingEdge;

WIU_InitStruct.WIU_Line = WIU_Line2;

WIU_Init(&WIU_InitStruct);

WIU_Cmd(ENABLE);

SCU_WakeUpLineConfig(2);

WIU_ClearITPendingBit(WIU_Line2);

WIU_ClearITPendingBit(2);

Other codes are also used for UART and RTC, they are working fine as interrupts.

Please ask if any more information or code is required.

Thanks and regards.

bbalasa
Associate II
May 17, 2011
Posted on May 17, 2011 at 09:58

GPIO3 generates INT on EXTIT0_ITLine.(WIU group0 VIC1.10)

Use EXTIT0_ITLine instead of EXTIT2_ITLine

satnam
satnamAuthor
Associate III
May 17, 2011
Posted on May 17, 2011 at 09:58

Thanks for the help, now it is working.