cancel
Showing results for 
Search instead for 
Did you mean: 

EVAL-RHF1201V2

Mo9
Associate

Hello. im currently using the EVAL-RHF1201V2 and would like some help setting it up to properly measure dynamic characteristics. Particularly regarding the RPOL resistance and for a sampling frequency of 40 Mbps and a differential AC input from 1 MHz to 10 MHz with a max amplitude of 2Vpp.

I also tried to apply the recommendations in the datasheet (fine = 15MHz and FS = 50 Mbps) in order to measure dynamic performance but I am far from obtaining them.

Can someone help me please?

 

1 REPLY 1
Peter BENSCH
ST Employee

Welcome @Mo9, to the community!

the EVAL-RHF1201V2 is a tool from the aerospace sector. As the community is primarily intended for mutual help between end users, nobody will be able to help you here.

However, I'd recommend you create a personal ticket with Online Support OLS.

Good luck!

Regards
/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.